Running an AI model in Low-Power?
Hi,
I'm working on an application on a STM32WB55 which is sampling sensor data with 52Hz and feed it into a Keras model. Both the raw sampling sensor data as the output of the model will be saved to external flash memory (every 64 samples). A 52Hz interrupt DRDY signal will trigger to start a sample. The device will sample the data for several hours a day. At the end of the day all data will be offloaded over BLE. So in the project the BLE stack is included as well. Now I wonder if I can add some low-power features to this project.
I would like to have some advice:
- My clock (HSE/ sysclock) are now running on 32 MHz. Is this something I can lower when running an AI model?
- Any advice on which mode is possible (like low-power RUN/SLEEP/STOP) ?
- Is it possible to shutdown CPU2 (BLE core) while CPU1 is running the AI code / sampling data?
I hope one of you can help me with one or more of above questions.
Thanks already!