SensorTile.box #10: ST.box main firmware function pack explained - overview
The purpose of the FP-SNS-STBOX1, which is the main functional pack (FP) dedicated to the ST.box, is to provide examples that show how to build custom applications for the Pro Mode at a FW level. Its flexibility allows the ease portability of this FP across different STM32 microcontrollers, so that you can build your customized app not starting from scratch.
The available pro-mode applications, a couple of which will be explained in the near future posts, are:
- BLEFOTA: uses ultra-low power implementation based on an RTOS for transmitting the data via BLE connectivity;
- BLELowPower: creates a BootLoader and an application for Firmware-Over-the-Air (FOTA) update;
- BLEMLC: programs the LSM6DSOX machine learning core for activity recognition or vibration monitoring and transmits the results via BLE;
- BLESensors: transmits sensor data in the simplest way for BLE trasmission;
- DataLog: saves the sensor data to the SD card (with FreeRTOS).
Together with these applications, there are also a couple of examples that involves other platforms:
- BootLoader: enables you to update the code;
- DataLogExtended: enables you to send data via USB and visualize the sensor data with Unicleo-GUI