Skip to main content
Explorer
February 17, 2026
Solved

ST Edge AI Core version in X-CUBE-AI

  • February 17, 2026
  • 2 replies
  • 169 views

Hello,

I am experimenting with X-Cube-AI (v10.2.0) in STM32CubeMX(v6.16.1). I noted that the version of the ST Edge AI Core in this case is v2.2.0. Moreover, this makes that the Embedded Interface is the legacy one, instead of the the newest ST-AI. I wonder if there are plans to update X-Cube-AI so it uses the latest version of ST Edge AI (v3.0.0), and uses the latest the ST-AI interface.

Thanks.

Best answer by Tuomas95

See this post, X-Cube-AI was replaced by STM32Cube AI Studio yesterday.

2 replies

Tuomas95Best answer
Associate III
February 19, 2026

See this post, X-Cube-AI was replaced by STM32Cube AI Studio yesterday.

Julian E.
Technical Moderator
February 19, 2026

Hi, 

Exactly, X Cube AI is no longer updated. It was replaced by STM32CubeAI studio, a desktop app.

You can use the ST Edge AI Core version 2.2 and later with it.

 

Make sure to update all the required dependencies.

 

Have a good day,

Julian

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.