ST Edge AI Dev Cloud Quantization not working
Hi,
I've been using ST Edge AI Dev Cloud to benchmark my human activity recognition models on some ST platforms and I would like to do the same for the STM32N6570-DK but it only accepts quantized models and the quantization option throws and error:
Executing with: {'model': '/tmp/quantization-service/0f29903b-6961-4c97-bde9-83219e06f56f/gmp_wl_24_human_activity_recognition_WISDM.h5', 'data': None, 'input_type': tf.float32, 'output_type': tf.int8, 'optimization': <Optimize.DEFAULT: 'DEFAULT'>, 'output': '/tmp/quantization-service/0f29903b-6961-4c97-bde9-83219e06f56f', 'disable_per_channel': False}
Invalid value for argument `reduction`. Expected one of {'mean', None, 'sum', 'none', 'sum_over_batch_size', 'mean_with_sample_weight'}. Received: reduction=auto
2025-07-31 09:19:58.238638: I tensorflow/core/util/port.cc:153] oneDNN custom operations are on. You may see slightly different numerical results due to floating-point round-off errors from different computation orders. To turn them off, set the environment variable `TF_ENABLE_ONEDNN_OPTS=0`.
2025-07-31 09:19:58.272098: I tensorflow/core/platform/cpu_feature_guard.cc:210] This TensorFlow binary is optimized to use available CPU instructions in performance-critical operations.
To enable the following instructions: AVX2 AVX512F AVX512_VNNI FMA, in other operations, rebuild TensorFlow with the appropriate compiler flags.
/usr/local/lib/python3.9/site-packages/keras/src/optimizers/base_optimizer.py:86: UserWarning: Argument `decay` is no longer supported and will be ignored.
warnings.warn(
I have tried both with my custom models and the ones built by ST, but none seem to work.
Important note is that quantization was working about 2 months ago, but then suddenly stopped.
Is there a fix for this?
Thanks in advance,
Best regards.