Solved
STM32 Cube AI studio E200(ValidationError): E801(HwIOError): Invalid firmware
- April 15, 2026
- 2 replies
- 100 views
Hello, I'm trying to create a project with custom model via STM32 Cube AI studio, which uses STedge Core AI v. 3.0.0. Validation is performed on STM32N6570-DK.
I'm getting following error:
E200(ValidationError): TARGET: Unable to bind the ST.AI runtime with "network" c-model: []
E801(HwIOError): Invalid firmware - COM7:115200 When running same command from command line I see that progress goes to 74,8 % and then stucks until error is displayed.
See attached failed report for details.