STM32 Model Zoo Help
I have followed the model zoo github tutorial to train, quantize and deploy an Audio Event Detection model. I used the available yamnet-256 and followed the tutorial to the end of deployment. I manage to get successful deployment but when I connect the B-U585I-IOT02A board, and open putty and connect via serial, i get this on putty:
Network informations...
model name : network
model signature : 0x80e2ec0fd41896ad70099555488edefd
model datetime : 2025-03-12T18:36:47+0800
compile datetime : Mar 12 2025 18:37:57
runtime version : 10.0.0
tools version : 2.0.0
complexity : 23932020 MACC
c-nodes : 21
map_activations : 1
[0] (1,1,1,112196)112196/u8 Q8.0 @0x20017480/112196
map_weights : 1
[0] (1,1,1,139176)139176/u8 Q8.0 @0x80201E0/139176
n_inputs/n_outputs : 1/1
I[0] (1,64,96,1)6144/i8 1:(0.053046,44), @0x20028180/6144
O[0] (1,1,1,10)10/float32 @0x2001748C/40
--- Start Processing ---
It stops at start processing, when I play the audio files from ESC-50 dataset, nothing happens. Am I supposed to perform some configurations on the stm32ide like enable the microphone or USART or something?