Question
STM32N6 Model zoo release 4.0
Hello,
- The latest version of X-CUBE-AI is 10.2.0, which comes with ST Edge AI Core v2.2.0.
- The latest Edge AI Core version is v3.0.0.
- The STM32 model zoo release 4.0 adds support for ST Edge AI Core v3.0.0.
- The STM32 model zoo release 3.2 adds support for ST Edge AI Core v2.2.0.
Some of the models from the model zoo release 4.0 fail to generate code with the latest X-CUBE-AI with errors such as "Your model ir_version is higher than the checker's".
What are the intended tools to build the models from the modelzoo 4.0 release for the STM32N6, or is only release 3.2 supported?
Thanks!