Skip to main content
Associate
August 28, 2023
Question

STWINKT1B Cloud Streaming and Predictive Maintenance

  • August 28, 2023
  • 1 reply
  • 1538 views

I am looking for a solution for a cohesive predictive maintenance application using continuous, real-time streaming of data that is continuously monitored for any changes. I was looking to use the industrial grade digital MEMS microphone (IMP34DT05), analog MEMS microphone with frequency response up to 80 kHz (IMP23ABSU) and/or ultra-wide bandwidth (up to 6 kHz), low-noise, 3-axis digital vibration sensor (IIS3DWB) on the STEVAL-STWINKT1B board. 


The goal is to have data continuously streamed via BLE or Wifi to the cloud, preferably AZURE. Whether it is though edge-processing (preferred) or any other data analysis, the end goal is to be able to continuously monitor this data and detect any anomalies or changes in the data that would indicate a maintenance issue. A possible audio application is FFT analysis and determining if a frequency is out of the expected range. 

From my understanding, X-CUBE-MEMSMIC1 and FP-SNS-DATALOG1 only have capabilities to collect / monitor data that has been saved to the SD card or streamed through USB. I am wondering if there is a way to incorporate X-CUBE-AZURE / X-CUBE-AZRTOS-L4 into the stand-alone/handmade projects in those software expansions to create a project I can modify for my own application after purchasing the STEVAL-STWINWFV1 board for Wifi compatibility.

Alternatively, I have looked into using FP-AI-MONITOR1 with either the X-CUBE-AI or NanoEdgeAI application. I am wondering which implementation would be better suited for continuous monitoring of the desired sensors. I have looked a bit at the X-CUBE-AI documentation but am not sure how to properly implement it yet.

I know ST supplies a function pack (FP-IND-PREDMNT1) that could potentially be useful in this scenario, but I am turned off by the need for DSH-PREDMNT and continuous payment for its use, and the inability to implement hand-made code in the project's execution.

Thank you.

This topic has been closed for replies.

1 reply

Federica Bossi
Technical Moderator
August 30, 2023

Hi @alars1 ,

Welcome to ST Community!

Your request is too general.
ST releases the different packages as examples but we do not have an example that perfectly matches your use case.

We do not provide direct support for customizing our solutions, but if you are not an experienced developer, we can refer you to one of our partners for support.

Let me know.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
alars1Author
Associate
August 30, 2023

Federica, 

Referral to a partner would be amazing. I appreciate your time on this matter. 

Thank you.