Skip to main content
Associate II
January 11, 2024
Solved

Unicleo-GUI not Detecting my NUCLEO-IKS01A3 Board

  • January 11, 2024
  • 2 replies
  • 1250 views

Hi all, 

I installed Unicleo-GUI on my Windows laptop, and was able to read sensor data from my NUCLEO-IKS01A3 board successfully. The board was automatically identified by the software as being connected to COM4 yesterday. For some reason today the software recognizes the COM connection but not the board and thus won't display the data being read by it on the screen. 

I have tried reinstalling Unicleo as well as the FP-SNS-DATALOG2 function pack with no success. 

Any advice or suggestions are appreciated!!

Best answer by Miroslav BATEK

The firmware from FS-SNS-DATALOG2 is not compatible with Unicleo-GUI. Compatible firmware is in X-CUBE-MEMS1 package.

2 replies

Miroslav BATEKBest answer
ST Employee
January 11, 2024

The firmware from FS-SNS-DATALOG2 is not compatible with Unicleo-GUI. Compatible firmware is in X-CUBE-MEMS1 package.

Federica Bossi
Technical Moderator
February 1, 2024

Hi @ZoeTakacs ,

Did you try to use the compatible firmware that Miroslav suggested you?

If yes, remember to click the 'accept as solution' button on his answer to be of help to other users :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.