Skip to main content
Evelina CAMILLERI
ST Employee
July 8, 2020
Question

What are the configurations that can be utilized when capturing data? And what are the limitations in terms of ODR and sensor configuration?

  • July 8, 2020
  • 1 reply
  • 579 views

 [webinar - Program decision trees in sensors with a Machine Learning Core]

This topic has been closed for replies.

1 reply

Evelina CAMILLERI
ST Employee
July 8, 2020

MLC can work at four different data rates: 12.5, 26, 52, 104 Hz. Data logs should be provided at one of these rates during the MLC configuration procedure. 

Besides these limitations, the sensor itself can work even at higher data rates, after the MLC has been configured, since the MLC will process data at its own rate. 

Together with MLC, also additional features (like filters, FIFO, FSM, etc..) can be configured on the sensor. When both FSM and MLC are enabled, a merge tool has to be used in Unico to generate a configuration including both features.