What's the newest ONNX Runtime version that the X-CUBE-AI 10.2.0 supports?
I want to train some small DL models with Nvidia's RTX 50 series GPU, which can work properly only with CUDA 12.x. I've learned that the CUDA 12.x is only compatible with ONNX Runtime 1.17.x or newer version. So I want to know if the X-CUBE-AI 10.2.0 support ONNX Runtime 1.17.x or newer version? If it can, I would like use the X-CUBE-AI 10.2.0 to deploy my DL models on the STM32 MCUs.