Skip to main content
TDK
Super User
December 19, 2025
Question

Attachment access and image viewing issues

  • December 19, 2025
  • 3 replies
  • 320 views

The "Virus scan in progress..." message is gone, but attachments are still behaving funny.

Issue 1: 2 out of the 3 attachments here cannot be accessed. Clicking on them does nothing and the "download" icon is missing.

https://community.st.com/t5/others-stm32-mcus-related/facing-difficulties-in-interfacing-stm32l433-mcu-to-vcnl4040-i2c/m-p/861339

TDK_0-1766113643986.png

 

Issue 2: I've also noticed that image attachments can't be viewed directly in the past week or so.

Trying to click on the png attached here shows an error instead of showing the image.

TDK_2-1766113825278.png

TDK_1-1766113792498.png

https://community.st.com/t5/stm32-mcus-products/stm32l433rct-freezing-lock-up-problem/m-p/865559/highlight/true#M290358

The download icon works and once downloaded the images can be viewed directly. They appear to be valid PNG files.

 

Seems forum functionality is going backwards. Split this to a new thread if you want. Seems related IMO.

3 replies

Lina_DABASINSKAITE
Community Manager
December 19, 2025

Thank you, @TDK , for sharing this information. I have escalated the issue to the troubleshooting team.
I apologize for the inconvenience in the meantime.

Best regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Andrew Neil
Super User
December 19, 2025

Yes, I have seen this recently.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
December 22, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.