Skip to main content
TDK
Super User
August 27, 2025
Question

"Latest reply" stats are sometimes incorrect

  • August 27, 2025
  • 1 reply
  • 336 views

Clicking on a user's name to view their profile, I can see their previous posts. For example:

TDK_1-1756326161630.png

It says the last reply to the thread was a week ago. However, when viewing that thread, there are 4 more replies after mine. The latest reply should reflect the last such reply.

 

How widespread is this problem? 2/4 of the posts from this user show a "latest reply" which is not the latest.

 

I viewed a few other user profiles and could find the same problem happening. Probably 25% or so are wrong. Here are a few:

TDK_2-1756326510752.png

TDK_3-1756326605411.png

 

1 reply

Lina_DABASINSKAITE
Community Manager
August 28, 2025

Hi @TDK,

Thanks for bringing this up!

To replicate this:

  • I checked now the profile of: @PKurz.1
  • But I see a different output then you. @TDK.

Lina_DABASINSKAITE_0-1756380378765.png

Questions:

  • Did you capture your screenshot on August 27, 2025, or earlier?
  • To define the urgency of this matter, can you share how often do you/or anyone else, use this component and for what use case?

I’ve raised this topic with our vendor to see if there are any issues with this component.
I will get back once I have news.  

Regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.