Skip to main content
TDK
Super User
August 22, 2024
Question

Missing option for strikethru text. Sometimes...

  • August 22, 2024
  • 2 replies
  • 2095 views

When editing a post, the strikethru (like this) style is missing. I clicked the area where the "..." should be to be sure there is no button. This is definitely a new bug. I could edit posts with strikethru before. Have noticed it a few times lately. Tried reloading the page. Nothing. Came back 15 minutes later and it shows up again. Re-looking at this screenshot of the issue that I took, maybe I should have clicked the "back" icon on the left? I don't know what that would do.

TDK_0-1724285601419.png

 

It's there when creating a post:

TDK_1-1724285636430.png

 

But it only happens sometimes. On other posts, it's clearly visible:

TDK_2-1724285699800.png

 

2 replies

Lina_DABASINSKAITE
Community Manager
August 22, 2024

Hello @TDK ,

Thanks for reporting this, good catch!

I need some more time replicate this, as I've tried a couple of times today and everything worked as expected. 

Can you please share the browser/version you are using? 

If anyone else is experiencing this, please let us now.

Thanks,
Lina

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
TDK
TDKAuthor
Super User
August 22, 2024

@Lina_DABASINSKAITE 

Win 11 Pro, Microsoft Edge Version 127.0.2651.105 (Official build) (64-bit). Should be whatever the latest updated version is.

I can't replicate it on demand either, but it has happened a few times. Don't think I'm doing anything special on my end. I turned off all browser extensions and it still happened. Not a big deal, but figured I would post it. Good luck. Shrug.

 

@Andrew Neil It was while editing my own reply I had made earlier to a post (to strikethru the bad info).

"If you feel a post has answered your question, please click ""Accept as Solution""."
Lina_DABASINSKAITE
Community Manager
August 23, 2024

Thanks @TDK , I will pass this info to investigate and inform when I have an update. 

Regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Andrew Neil
Super User
August 22, 2024

Is that "editing" while creating a new post, or going back to an existing post?

Is it editing your own post, or someone else's?

 

 

 

Some test text to play with

^^^ I went back to edit that ^^^

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.