Skip to main content
Andrew Neil
Super User
February 14, 2024
Question

multiple notifications for the same post

  • February 14, 2024
  • 1 reply
  • 1009 views

These two notifications refer to the exact same post:

AndrewNeil_0-1707917580502.png

He couldn't have mentioned me without making a reply, so I really don't need two separate notifications!

EDIT

And why are the two email notifications sent 7 minutes apart?!

AndrewNeil_0-1707917914560.png

 

    1 reply

    Laurids_PETERSEN
    Community Manager
    February 19, 2024

    Hi @Andrew Neil,

    Thanks for your feedback. 

    Given that the notifications are triggered separately there is no immediate fix/workaround to this issue. 

    We can look into scenarios where only one notification is necessary in general. I can't promise we can change anything soon, but the feedback is noted. 

    Best regards,
    Laurids 
     

    Andrew Neil
    Super User
    July 31, 2024

    @Laurids_PETERSEN wrote:

    the notifications are triggered separately the


    Why?

    Here we see that notifications can be combined:

    https://community.st.com/t5/feedback-forum/notification-feed-corrupted/m-p/703905/highlight/true#M1597

    @Lina_DABASINSKAITE 

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.