Skip to main content
Lead II
July 22, 2024
Question

Notification feed corrupted

  • July 22, 2024
  • 3 replies
  • 1312 views

This notification is incorrect. This user created a new topic and did not reply in this topic:

Schermafbeelding 2024-07-22 165515.png

 

This notification is also incorrect:

Schermafbeelding 2024-07-22 165449.png

Two unrelated notifications got merged. I saw this happen once before and I was confused about it.

I use Firefox.

3 replies

Andrew Neil
Super User
July 22, 2024

I think the notifications go wrong like this when those with the powers do things like editing, moving, marking solutions, etc

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Lina_DABASINSKAITE
Community Manager
July 26, 2024

Hello @unsigned_char_array ,

Thanks for sharing your feedback. As Andrew mentioned, the notifications are inconsistent whenever our expert does content management. The return "posted a new topic" actually means that Amel moved a topic in a new location. However, the "replied to the topic" one, I need to clarify when it happens exactly.  I will share as soon as I clarify this. 

Greetings,
Lina

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Lina_DABASINSKAITE
Community Manager
July 31, 2024

I double check and regarding this: 

This notification is also incorrect:

Schermafbeelding 2024-07-22 165449.png

Two unrelated notifications got merged. I saw this happen once before and I was confused about it.

I use Firefox.


Please check the original thread here: Out dated conventional circuit techniques still used by ST Microelectronics!.

you responded there and by posting the comment you have subscribed to updates about this thread.

TDK and SofLit  posted their comments after you so you were notified about this fact. Since both posts were in this thread, you received a merged notification with the following comment: "replied to topic". This is expected behavior. 

Let me know if it is clear. 

Regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Andrew Neil
Super User
July 31, 2024

@Lina_DABASINSKAITE wrote:

Since both posts were in this thread, you received a merged notification 


So it can combine notifications!

Why, then, do we get this:

https://community.st.com/t5/feedback-forum/multiple-notifications-for-the-same-post/m-p/639727#M1035

@Laurids_PETERSEN 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.