Should I be reporting AI-generated nonsense responses?
In instances where they don't answer the question, or where they answer it incorrectly, I have been reporting these. Should I keep doing so?
Does the ST community have a stance on whether or not AI-generated reponses are allowed? Is that stance in the guidelines and if not, can we put it there?
For example, clearly this is ChatGPT generated nonsense:

Another one, same thread even.

At first glance it seems like these answer the question, but they fall apart under inspection. These two are obvious, some are less so.