Cannot enable the autonomous STAGPS engine on TESEO-LIV3R
I have a Teseo LIV3R on a breakout board connected (via UART) to Tesio Suite. I'm trying to figure out how to enable STAGPS and test its functionality. Unfortunately I cannot enable the autonomous STAGPS engine using the command:
$PSTMSTAGPSONOFF,1
When sending the command $PSTMSTAGPSONOFF,1 to the module, I get no response. I would expect a response such as $PSTMPOLSTARTED. When sending the command $PSTMCFGAGPS,1 I get a response that the AGPS engine has been enabled. I would like to enable the autonomous STAGPS functionality though but I am not able to.
Hopefully someone canhelp or have an idea what the problem is?
Also, I was not able to confirm if the autonomous STAGPS function is enabled as default. Does anyone know if it is, and how to confirm this?
Thanks in advance.