Skip to main content
AAl S.1
Associate III
June 11, 2020
Solved

Hi, I want to connect Teseo-Liv3R to an active antenna. I have seen in the Data sheet section number 6.2 how to connect it. My questions:

  • June 11, 2020
  • 1 reply
  • 1220 views

1- What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?

2- I have seen in the   in section 7 general schematic. Is it for passive antenna only?

Thanks

best regards

    This topic has been closed for replies.
    Best answer by Francesco Virlinzi

    > What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?

    fig.10 and Fig11 are similar. In the second case (fig.11) the switch works also as current limiter

    There is a type in the image S22943 stands for TPS22943.

    >2- I have seen in the   in section 7 general schematic. Is it for passive antenna only?

    Yes.

    Regards

    Francesco

    1 reply

    Technical Moderator
    June 29, 2020

    > What is the deference between figure 10 and 11? And what is (S22943) in figure 11? is all I need to use active antenna inductor and capacitor? If it is yes what is the value?

    fig.10 and Fig11 are similar. In the second case (fig.11) the switch works also as current limiter

    There is a type in the image S22943 stands for TPS22943.

    >2- I have seen in the   in section 7 general schematic. Is it for passive antenna only?

    Yes.

    Regards

    Francesco