LIV4F less sensitivity compared to MAX-M10S?
Hi all,
to evaluate LIV4F and MAX-M10S, I use Mikroe "GNSS 9" and "MAX" click boards with a passive antenna (Quectel YEGT001W1AM).
While the MAX click board with the MAX-M10S gets a fix in less than one minute, the MAX 9 board with the LIV4F doesn't get a fix. Even when starting with an active antenna to get a fix and then switching to the passive antenna, the LIV4F stops operating. Sporadically, the GSV sentence shows then one or two weak (~20) signals while the MAX-M10S has >10 satellites with signals in the range 20..44.
From my understanding of the data sheets, both the LIV4F and MAX-M10S should have similar performance without an external LNA, isn't it?
Is there any known issue with the Mikroe GNSS 9 click board?
Or a possible misconfiguration of the LIV4F I could fix?