LIV4F reserved pin 7
Hello,
I have a design with same pinout and package (as LIV4F) that is working with 3.3V from other vendor.
Pin 7 is used as VCC_IO and it is connected to 3.3V.
The question is, can I replace and put the LIV4F instead?
What will happen if pin 7 will get 3.3V (instead of being not connected)?
Any chance of harm or malfunction?
I don't expect logic issue since I'm working with 3.3V anyway (and no conflict with past pin configuration that was VCC_IO)