Skip to main content
Associate
September 13, 2023
Question

STA8100-EVB-T5DR question

  • September 13, 2023
  • 2 replies
  • 1774 views

"I would like to ask a few questions:

  1. Initially, I was able to use the EVB-T5DR, and the NMEA decoding displayed information correctly. However, for some reason, it suddenly stopped working. When I used the UART tool to read the data, it appeared as Garbled code. How can I resolve this issue?

  2. iverson3ya_0-1694571394749.png

  3. Due to the problem mentioned in the first point, I decided to reflash the device, but I encountered a 'sync error' and couldn't flash it.

  4. iverson3ya_1-1694571553602.png

I would appreciate your help with the above two issues. Thank you.

This topic has been closed for replies.

2 replies

Issamos
Lead III
September 13, 2023

Hello @iverson3ya 

I suggest you:

For the 1st part to follow these steps:

Screenshot_2023-09-13-07-59-14-50_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

Screenshot_2023-09-13-07-58-47-37_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

for the second, you should follow those steps:

Screenshot_2023-09-13-07-58-16-15_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

Best regards.

II

Associate
September 14, 2023

I have followed these steps to burn the disc, but it still shows a 'sync error'.

Technical Moderator
September 28, 2023

Try following these steps:

  1. On the board push and maintain the left (BOOT) white bottom
  2. On the board push and release the right (Reset) white bottom
  3. On Teseo-Suite - T5 Xloader panel - Push 'Start' button

Regards

 Francesco

Technical Moderator
September 28, 2023

Hi

I see you were installing a new firmware.

Could I ask which firmware and which patch (scenario) you were installing?

I think you installed some 'RTCM based scenario' and now the STA8100 is senting RTCM (binary) data.

Regards

 Francesco