Skip to main content
jg_spitfire
Senior
April 22, 2020
Solved

Teseo-LIV3F vs STA8089FG why the module is shielded and the IC is unshielded?

  • April 22, 2020
  • 4 replies
  • 1653 views

Hi, I have been reading about this module (Teseo-LIV3F) and this IC (STA8089FG), as I can see both offers almost the same characteristics and both need external circuits to connect an antenna, so in which case should I use one or another?, why the module is shielded and the IC is unshielded?, I thought that all the RF components must be shielded but this is a case where I think I was wrong

Thanks

    This topic has been closed for replies.
    Best answer by Francesco Virlinzi

    Added to what Clive already said you have also to take into account that:

    • STA8089FG isn't a final product; it's just a chip which needs extra components to be used. Due to that ST doesn't care on legal certification to stay on the market (these certification have to be managed by the final producer)
    • Teseo-LIV3F is a final product ready to be used. with just a battery and it works... due to that it has to follow mandatory European and USA certification (ETSI and FCC) to stay on the market. To follow this certification shield is mandatory.

    At the end....

    If you use Teseo-LIV3F certification are already managed by ST, while if you use STA8089FG you will have to manage shield and certification on your own.

    Hope this helps

    Regards

    Francesco

    4 replies

    Tesla DeLorean
    Guru
    April 22, 2020

    With the IC you're expected to design the board and provide shielding. You need to pay attention to your supplies, and routing clocks and GPIO away from the IC.

    The IC generates local copies of code/carrier, and then correlates over several milli-seconds, the GNSS signals are buried in the noise floor. It is going to have some sensitivity to switching noise in the IF of the baseband processing, similar signals will look like jammers. Given you're generating a lot of frequencies internally, you don't want to be radiating those either.

    Unless you're doing 100K+ units I don't suppose ST is going to support you in an IC-Down implementation.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    jg_spitfire
    Senior
    April 28, 2020

    Hi, it makes sense (shield the IC), but look at this https://www.mikroe.com/gnss-zoe-click, if shielding is a requirement why do they put that GNSS module (U1) unshielded? , is very strange, someone told me that they do this to make a cheap product and also said that with the appropiate PCB design you can avoid the EMI, what do you think about this click board?

    Technical Moderator
    April 23, 2020

    Added to what Clive already said you have also to take into account that:

    • STA8089FG isn't a final product; it's just a chip which needs extra components to be used. Due to that ST doesn't care on legal certification to stay on the market (these certification have to be managed by the final producer)
    • Teseo-LIV3F is a final product ready to be used. with just a battery and it works... due to that it has to follow mandatory European and USA certification (ETSI and FCC) to stay on the market. To follow this certification shield is mandatory.

    At the end....

    If you use Teseo-LIV3F certification are already managed by ST, while if you use STA8089FG you will have to manage shield and certification on your own.

    Hope this helps

    Regards

    Francesco

    jg_spitfire
    Senior
    April 28, 2020

    Hi, I have read about the shield and certification and I understand that, but as I mentioned before both needs external components, so the unique difference would be the certification right?, the 7.1 schematic is a photo from the TESEO module hardware manual, even it seems that TESEO needs more external components than the STA8089 (figure 30), because it mentions that you need an external SAW filter and LNA, and the STA8089 has internal LNA and does not mention any time that a SAW is needed, just needs a few components for the antenna detection, or maybe am I wrong?, thanks

    0693W000000WZdMQAW.jpg

    0693W000000WZZZQA4.jpg0693W000000WZWzQAO.jpg

    Technical Moderator
    April 28, 2020

    Hi Jairo

    Teseo-LIV3F is a product ready for Mass-Market. It has reduced pin-out and we can support it also in case of low volumt.

    STA8089FG is a chip which wants high valume to be supported.

    Regards

    Francesco

    STLearner
    Associate III
    December 19, 2022

    Hi Francesco,

    Would like to check if the Teseo-LIV3F has certification for Australia/New Zealand market?

    Thank you.