TESEO-LIV3R standby command not working
Hi, I have a EVB-LIV3R board and I'm trying to command its power modes.
To put the device on standby mode, it is declared that we can use the "#PSTMFORCESTANDBY,<time>" message, where <time> is the number of seconds (see UM2523). But when I try to do it, the device goes asleep indefinitely, and also doesn't respond to any input on the Wakeup Pin (pin#5 on chip, available on test point #310 labelled on board).
Am I missing something? Do I have to configure the device with other commands before it? Why do the wakeup pin can't achieve it's purpose?