Teseo-LIV4F wakeup, interrupt, and nReset confusion
It is unclear to me how to place the Teseo-LIV4F to a low power state. I am a bit confused with the nReset and the Wakeup or Extint pins. In the datasheet, pin 5 is marked as an input and named "WakeUp" and pin 9 is marked as an input and named nReset. Pin 18 is also an input and is named PRG but its description says "Program or WakeUp from DeepStandby. What is DeepStandby?
The Teseo-LIV4F has a $PSTMFORCESTANDBY command and the datasheet lists a SW-STANDBY consumption of 10uA with VCC=VBAT=3.3V (which is great for me) but the Hardware Manual says "Teseo-LIV4F offers 1 way of standby: HW standby".
What is the best way to enter and exit standby with VBAT at 3.0V and VCC also at 3.0V? Or is it better to just control VCC?