Teseo V EVB-T5DR Teseo-Suite NMEA uart port connect
- October 24, 2024
- 1 reply
- 1661 views
Hi,
Can you help me to confirm the difference between ST Teseo-Suite Pro uart com port connect and normal com port software Tera Term connect?
I have confirmed that the baudrate settings are the same, and the Teseo-Suite software com port connect behavior does not have any uart output.
Teseo-Suite software com port connect behavior does not have any uart output problem:
Using Teseo-Suite software connect can capture NMEA data stream.
When I use Tera Term to connect EVB-T5DR E1, all signal light will go out.
Is it necessary to send a specific command to EVB-T5DR E1 or is it necessary to adjust the hardware?
Please clarify.
The following is the verification procedure:
1. Use com0com software to create two virtual uart com ports, com 3 to receive and com 4 to output (com0com.png).
2. Run import serial.py to listen to com 4 to display all uart commands received by com 3 (comport.png).
3. Teseo-Suite software clicks connect, no uart command is displayed (teseo.png)
4. Teseo-Suite software click Execute NMEA script to output uart setup command (teseo.png)
5. import serial.py shows all uart commands received by com 3 (comport.png)
Thank you for your help.