Skip to main content
Xynium
Associate III
October 12, 2020
Question

UM2229 Rev 4 missing details

  • October 12, 2020
  • 2 replies
  • 764 views

HI,

in UM2229 rev4 bottom of page 86/239 it seem value are missing in front of decription "Constellation disabled, Constellation satellites only tracked, Satellites constellation used in position evaluation"

This topic has been closed for replies.

2 replies

Technical Moderator
October 13, 2020

Hi.

You are right, I'l take note to fix it in the next version:

FYI:

0; Constellation disabled;

1: Constellation satellites only tracked;

2: Satellites constellation used in position evaluation

Regards

Francesco

Xynium
XyniumAuthor
Associate III
October 13, 2020

Ok Tks

 may be an error page 192/239  "Enable/disable the usage of RTC from the GNSS engine. It is recommended to have RTC

usage disabled (Bit12 set to 1) is the RTC crystal is not mounted"

should be (Bit12 set to 0) if disabled or 1 if enabled