Skip to main content
Associate II
February 24, 2025
Question

VIC3DA Dead reckoning not working

  • February 24, 2025
  • 1 reply
  • 2685 views

 

I have some problem with DR mode.

I can't recieve any $PSTMDR2 or $PSTMDRCAL messages, so the status of DR remains unknown.

But I checked the CDB 228-230 with $PSTMGETPAR, the following are the response.

========

$$PSTMSETPAR,1228,0x00000000*5A
$$PSTMSETPAR,1229,0x6cc22000*5D
$$PSTMSETPAR,1230,0x00000000*53

==========

In CDB 229, bit 60-63 is 6, meaning that the $PSTMDR and $PSTMDRCONFID are enabled, but I can only see $PSTMDRCONFID. There are no $PSTMDR message there. Are there any problem with my configurations?

Also, I had enabled these messages in CDB 229, meaning that these message should be update in 10 Hz. But it still be updated in 1 Hz, as following.

==========

$$PSTMDRCONFID,0.00,0.00,0.0000,0.0000,0.00,0.0000,0.000000,0.000000,0.0000,0.0,0.0,-0.0,0.0*1A
$$PSTMDRPVA,162640.000,2945690305,37.5517719,14.2984835,730.1,0.00,0.00,0.00,0.00,0.00,0.00*57
$$PSTMDRCONFID,0.00,0.00,0.0000,0.0000,0.00,0.0000,0.000000,0.000000,0.0000,0.0,0.0,-0.0,0.0*1A
$$PSTMDRPVA,162641.000,2946713305,37.5517719,14.2984835,730.1,0.00,0.00,0.00,0.00,0.00,0.00*5F
$$PSTMDRCONFID,0.00,0.00,0.0000,0.0000,0.00,0.0000,0.000000,0.000000,0.0000,0.0,0.0,-0.0,0.0*1A
$$PSTMDRPVA,162642.000,2947736306,37.5517719,14.2984835,730.1,0.00,0.00,0.00,0.00,0.00,0.00*59
$$PSTMDRCONFID,0.00,0.00,0.0000,0.0000,0.00,0.0000,0.000000,0.000000,0.0000,0.0,0.0,-0.0,0.0*1A
$$PSTMDRPVA,162643.000,2948758283,37.5517719,14.2984835,730.1,0.00,0.00,0.00,0.00,0.00,0.00*53

=========

Are there some configurations needs to be changed? Thank you.

1 reply

Technical Moderator
February 26, 2025

Hi,

CDB-228 contains all the $PSTMDR messages, so having values all 0s explains why you are not seeing any PSTMDR messages.

Can you please refer to $PSTMSETPAR command on how to set the bits. It looks like you might have overwritten the CDB registers.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
yclinAuthor
Associate II
March 3, 2025

Hi @GalaxyQuest 

Thank you for your response. I had understood that these DR messages report at 1 Hz, so these message should be set in CDB 228 (that include 1 Hz messages)

Also, I can recieve these DR messages after a factory reset. Just a note if someone needed.

CDB 228: 0x6cc22000   CDB 229: 0x0 CDB 230: 0x0

CDB 600: 80A00116 (there is a conflict that the manual says the bit 31 should be 0, but the default setting is 1)

=================

My new question is how to improve the DR performence?

I followed the instructions written in AN5678, and I got "system ready" flag.

I tested DR in a 2 km tunnel. But when I leave the tunnel, the position shift 500 m when the GPS was available.

Are there some values that I can know the accuracy of the DR? like the error in PSTMDR2?

Thank you.

Technical Moderator
March 3, 2025

Hi,

Couple of things to check.

I am assuming you are using DRUM mode -- i.e. no connections to vehicle, is that correct?

If so, in PSTMDR2 - you should see SYSTEM_READY along with status of 0xCC should be seen in IMU cal.

0xCC means accelerometer calibration and gyro calibration is completed.

Secondly,

Could you please ensure that when doing field testing, the device is firmly placed on the vehicle frame and not placed on a seat where it can move around?

 

Regarding DR messages.

In PSTMDR2 we report the cross track and along track error which is a good reference.

In addition, we also report PSTMDRPVA - which is DR estimated position and PSTMDRGPS - which is pure GNSS.

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.