What are the differences in connecting with Teseo Suite and Terminal software?
Hello,
I am able to receive data normally when connecting USB with Teseo Suite, but when I connect using Terminal software, there is no data output at all. I am sure the baud rate is 460800. Is there a specific command I need to input for it to start outputting data?
I am using "Teseo EVB".
The connection with Teseo Suite is normal, and the data output is also normal:

However, when I use Terminal software to connect, there is no data output at all:
Is there a specific command I need to input for it to start outputting data?

Thank you.