Skip to main content
Technical Moderator
May 24, 2018
Question

www.st.com

  • May 24, 2018
  • 1 reply
  • 10035 views

FAQ on Teseo-LIV3F

Q) Where can I find information on Teseo-LIV3F

A) All the information are available on-line on www.st.com

 Q) Which constellations are supported on Teseo-LIV3F?

A) Teseo-LIV3F supports GPS, Glonass, Galileo, BeiDou and QZSS constellations

Q) How many channel does Teseo-LIV3F use?

A) Teseo-LIV3F uses at least 32 channels; SBAS takes at least 4 channels for each system (these values are fixed during firmware generation and can not be modified)

Q) Which are the maximum velocity and altitude Teseo-LIV3F can guarantee to continuously update its position?

A) Teseo-LIV3F has to be ITAR limits compliant which are:

  • speed: 515 m/s
  • altitude: 18000 [m]

when both the condition are true the Teseo-LIV3F stops providing the PVT solution.

In any case the absolute Teseo-LIV3F limits are:

  • speed: 600 m/s
  • altitude: 100000 [m]

Q) Does Teseo-LIV3F support Assisted GNSS?

A) Yes. It does. Teseo-LIV3F support three Assisted GNSS:

  1. ST-AGNSS (no internet connection needed)
  2. Predictive AGNSS (internet connection needed) and
  3. RealTime-AGNSS (internet connection needed)

Q) Does Teseo-LIV3F support Raw Measurement data?

A) No it doesn't

Q) Should I write Teseo-LIV3F driver from scratch?

A) No you shouldn't. ST provides ready-to-be-used device driver on:

Q) Is there an evaluation board?

A) Yes. There is the Teseo-LIV3F evaluation board. Further information on www.st.com

Q) Why PVT solution isn't provided when 4 satellites are seen?

GNSS algorithm needs 4 satellites to evaluate PVT solution, but they have to be good satellites; if under specific thresholds a satellite can be rejected in the PVT solution.

These thresholds can be modified:

  • CDB-ID 132 – GNSS Positioning CN0 threshold
  • CDB-ID 198 – GNSS Mask angle positioning

Q) Is there a prototyping board?

A) Yes. There is the X-Nucleo-GNSS1A1 the Teseo-LIV3F prototyping board. Further information on www.st.com

Q) Is there an evaluation software PC tool?

A) Yes. There is the Teseo-Suite PC tool available on www.st.com

Q) Is there minimal order quantity?

A) No there is no minimal order quantity.

Q) Can the Teseo-LIV3F be re-programmed?

A) Yes, it can. Teseo-LIV3F supports firmware update on the field.

Q) Can the Teseo-LIV3F host customer-application/code?

A) No it can not. There is no SDK available on Teseo-LIV3F. Teseo-LIV3F isn't an open platform. It can be reprogrammed only with binary provided by ST

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    June 9, 2018
    Posted on June 09, 2018 at 13:58

    Been trying to find anyone selling the X-NUCLEO-GNSS for a month, is it in stock anywhere? When should we expect to see stock?

    https://community.st.com/0D50X00009XkgXZSAZ

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..