X-NUCLEO-GNSS1A1: Using the LIV3F Receiver with Teseo Suite
I have recently procured a X-NUCLEO-GNSS1A1 on its own. I would simply like to use the LIV3F to test the LNA/SAW filtering along with different antennas as well. I am able to connect the LIV3F to Teseo Suite via FTDI -> UART. I can see all of the satellites and NMEA data being streamed by the receiver, but I am unable to change any settings. I need to update a couple of settings, but the LIV3F is not detected, and it is shown in Teseo Suite as a 'generic' device, instead of a LIV3F, or LIV3FL, etc.
Any assistance would be much appreciated, I feel that I've exhausted every resource I have trying to change the settings. fwiw, I have a couple of custom PCBs with LIV3Fs installed on them, and I do not have this issue with those boards. Only the LIV3F on the X-NUCLEO-GNSS1A1.