Skip to main content
PNadar08
Associate
February 27, 2021
Question

Can the People Count data be sent from VL53L1X Sensor using Wifi ? How to integrate the Wifi Module? Also what changes have to be made in the Source Code of VL53L1X People Count for the same?

  • February 27, 2021
  • 1 reply
  • 637 views

I need to send the People count obtained from VL53L1X to the Server using Wifi. Does STM32 connect to Wifi or do we need an external Wifi Module for this? Also what changes have to be made in the VL53L1X code and also in which .c file of src/API folder those changes need to be implemented so that the count can be sent using HTTPS to the Server.

This topic has been closed for replies.

1 reply

Jmigu.1
Associate
March 18, 2021

+1, i'm having the same question