Comparison of features of various ToF Sensors
I'm a little frustrated that there isn't a "Here's ST's Time of Flight sensor offering and which sensors have which features" kind of page. The sensor datasheets themselves also do not give any real comparison data to other (pin compatible) parts.
From what I have gathered:
vl53l0x - 25o FOV, base model in ranging sensors. Single zone, single target
vl53l1 - 27o FOV, multi-zone (adjustable FoV)
vl53l1x - same but with more zones?
vl53l1cb - no idea
vl53l2 - not a product
vl53l3cx - 25o FOV, multi target, faster (1MHz) I2C
vl53l4cd - 18o FOV, short range (1mm - 1300mm), fast (100Hz), 1MHz I2C
vl53l4cx - histogram based (?), long range (0-6000mm), 18o, multi target
Looks like the L5 isn't footprint-compatible:
vl53l5cx - 63o FOV, multizone, mutli-target
vl53l5cp - cx + person detect?
vl53l8ca - 2nd gen, wide FOV like L5, pin compatible with L5?
Then there's the VL6180, which is not footprint compatible and I think is older, based on an earlier ToF design, and the VL6180x which adds an ALS?
I also found John Kvam's presentation on ToF sensors (is there a video of the webinar that goes with the slides?) but it also does not go into the differences between these products and when/how to choose one over another.