Difference Between A and B Message
I've seen references to various A and B or (even and odd) messages for the ToF sensors.
In my application, it turns out that every other measurement is not great, so if I throw out packets based on their message ID count, then I get perfect data but at half measurement rates. The effect I see is that the measurements oscillate between the real value and a nearby (within 6 or 10cm) value.
I think for my sensor, the packet that contains the ambient data is the better one.
Is there more documentation on what the two packets are and why the measurements would be different between the two? Is there a way to set them both to operate the same so that I don't lose half the samples?