Visitor II
July 27, 2022
Question
Does the angle of the target create problems with the VL53L4CX sensor?
- July 27, 2022
- 1 reply
- 882 views
I am considering using the above sensor to detect if a car is in a parking space in a garage. I would plan to mount the sensor ~6' above the floor on the wall at the end of the space. It would be pointing down in a 45˚ angle, which means the center of the FOV would be ~6' horizontally from the wall. Will this angle of viewing the floor be a problem? Obviously, when a vehicle is in the space, the measured distance would be much less. That's the fundamental concept of this detection method.