Skip to main content
Visitor II
February 1, 2024
Solved

Error compiling ToF sensor drivers on Linux - VL53L4CX

  • February 1, 2024
  • 1 reply
  • 1272 views

I am trying to compile the drivers for the ToF sensor: VL53L4CX for an embedded Linux application. I am running Ubuntu 22.04. When I try to make the drivers I get the following error:

 

 

 

CONFIG_STMVL53LX=m make -C /lib/modules/`uname -r`/build M=$PWD
make[1]: Entering directory '/usr/src/linux-headers-6.5.0-15-generic'
warning: the compiler differs from the one used to build the kernel
 The kernel was built by: x86_64-linux-gnu-gcc-12 (Ubuntu 12.3.0-1ubuntu1~22.04) 12.3.0
 You are using: gcc-12 (Ubuntu 12.3.0-1ubuntu1~22.04) 12.3.0
 CC [M] /home/USERNAME/programs/VL53L4CX_LinuxDriver_1.1.2_bare_1.2.8/driver/vl53Lx/stmvl53lx_module-i2c.o
/home/USERNAME/programs/VL53L4CX_LinuxDriver_1.1.2_bare_1.2.8/driver/vl53Lx/stmvl53lx_module-i2c.c:567:19: error: initialization of ‘int (*)(struct i2c_client *)’ from incompatible pointer type ‘int (*)(struct i2c_client *, const struct i2c_device_id *)’ [-Werror=incompatible-pointer-types]
 567 | .probe = stmvl53lx_probe,
 | ^~~~~~~~~~~~~~~
/home/USERNAME/programs/VL53L4CX_LinuxDriver_1.1.2_bare_1.2.8/driver/vl53Lx/stmvl53lx_module-i2c.c:567:19: note: (near initialization for ‘stmvl53lx_driver.<anonymous>.probe’)
/home/USERNAME/programs/VL53L4CX_LinuxDriver_1.1.2_bare_1.2.8/driver/vl53Lx/stmvl53lx_module-i2c.c:568:19: error: initialization of ‘void (*)(struct i2c_client *)’ from incompatible pointer type ‘int (*)(struct i2c_client *)’ [-Werror=incompatible-pointer-types]
 568 | .remove = stmvl53lx_remove,
 | ^~~~~~~~~~~~~~~~
/home/USERNAME/programs/VL53L4CX_LinuxDriver_1.1.2_bare_1.2.8/driver/vl53Lx/stmvl53lx_module-i2c.c:568:19: note: (near initialization for ‘stmvl53lx_driver.remove’)
cc1: some warnings being treated as errors
make[3]: *** [scripts/Makefile.build:251: /home/USERNAME/programs/VL53L4CX_LinuxDriver_1.1.2_bare_1.2.8/driver/vl53Lx/stmvl53lx_module-i2c.o] Error 1
make[2]: *** [/usr/src/linux-headers-6.5.0-15-generic/Makefile:2037: /home/USERNAME/programs/VL53L4CX_LinuxDriver_1.1.2_bare_1.2.8/driver/vl53Lx] Error 2
make[1]: *** [Makefile:234: __sub-make] Error 2
make[1]: Leaving directory '/usr/src/linux-headers-6.5.0-15-generic'
make: *** [Makefile:8: default] Error 2

 

 

 

 

It seems that I am using a very similar but slightly different compiler version, but I wouldn't think that it should matter as its the same major version. I am getting a type error within the driver code.
Does anyone know how I can remedy this? I can't seem to find this x86_64-linux-gnu-gcc-12 version to try it with.
Thanks for your help

This topic has been closed for replies.
Best answer by John E KVAM

Installing drivers into the Kernel is not for the faint of heart. 

But do you need to?

If you are building something where you don't want some user's code to gain access to the I2C bus then you have to create a kernel driver.  

But if you don't allow user code onto your system, you can run the sensor as a user app and bypass this problem. 

The job of the kernel driver is to make it so a user application can access the VL53L device via i2c with exposing other devices on that bus. The kernel can verify that the transaction is valid and talking to a legitimate device - as opposed to trying to read system EEPROM or something. 

User apps are a lot easier - just download the API from ST.com and make the platform.c functions work for Linux. Or you can simply search GitHub for Linux applications. They will have working Platform.c files.

That code was verified on a Raspberry Pi, and different versions of Linux are going to be slightly different. 

I googled "ubunto struct i2c_client" and saw several articles that might shed some light on the issue. 

Sorry I cannot help more.

- john

 

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
February 1, 2024

Installing drivers into the Kernel is not for the faint of heart. 

But do you need to?

If you are building something where you don't want some user's code to gain access to the I2C bus then you have to create a kernel driver.  

But if you don't allow user code onto your system, you can run the sensor as a user app and bypass this problem. 

The job of the kernel driver is to make it so a user application can access the VL53L device via i2c with exposing other devices on that bus. The kernel can verify that the transaction is valid and talking to a legitimate device - as opposed to trying to read system EEPROM or something. 

User apps are a lot easier - just download the API from ST.com and make the platform.c functions work for Linux. Or you can simply search GitHub for Linux applications. They will have working Platform.c files.

That code was verified on a Raspberry Pi, and different versions of Linux are going to be slightly different. 

I googled "ubunto struct i2c_client" and saw several articles that might shed some light on the issue. 

Sorry I cannot help more.

- john