error with vd66gy on Raspberry Pi
Hello everyone, i'm trying to use the vd66gy with the raspbeery Pi x64 connected on cam0 and im following all the steps of the "Linux Start Guide for ST BrightSense" but it still doesnt work. I downloaded the drivers for the camera as well as the libcam st version from this link: https://www.st.com/en/embedded-software/stsw-img503.html?dl=redirect. However i see that even for the vd66gy driver, the en.vd66gy_1.0.3.zip has all the vd56g3 files and the makefile looks like this:
ifneq ($(KERNELRELEASE),)
include Kbuild
else
KVERSION ?= `uname -r`
KDIR ?= /lib/modules/${KVERSION}/build
default:
CONFIG_DRIVER_VD56G3=m $(MAKE) -C $(KDIR) M=$$PWD
clean:
CONFIG_DRIVER_VD56G3=m $(MAKE) -C $(KDIR) M=$$PWD clean
endifIs this a mistake? It looks like the vd56g3 driver. You can confirm by downloading the driver from the link. As a result when i complete all the steps and launch rpicam-hello i get this:
rpicam-hello
[0:30:33.792539716] [3479] INFO Camera camera_manager.cpp:327 libcamera v0.0.0+5323-a9c0f393-dirty (2025-02-17T12:13:30UTC)
[0:30:33.800260593] [3482] INFO RPI pisp.cpp:720 libpisp version v1.1.0 e7974a156008 27-01-2025 (21:50:51)
[0:30:33.801208462] [3482] WARN CameraSensorProperties camera_sensor_properties.cpp:473 No static properties available for 'vd56g3'
[0:30:33.801220202] [3482] WARN CameraSensorProperties camera_sensor_properties.cpp:475 Please consider updating the camera sensor properties database
[0:30:33.810869132] [3482] ERROR IPAProxy ipa_proxy.cpp:154 Configuration file 'vd56g3.json' not found for IPA module 'rpi/pisp'
[0:30:33.811002317] [3482] WARN RPiController controller.cpp:91 Failed to open tuning file ''
[0:30:33.811015076] [3482] ERROR IPARPI ipa_base.cpp:152 Failed to load tuning data file
[0:30:33.811028688] [3482] ERROR RPI pipeline_base.cpp:814 Failed to load a suitable IPA library
[0:30:33.811040428] [3482] ERROR RPI pisp.cpp:947 Failed to register camera vd56g3 10-0010: -22
Made X/EGL preview window
ERROR: *** no cameras available ***Is the driver for the vd66gy anywhere else to download?
error msgs and data of the en.vd66gy_1.0.3 file which contains the vd66gy driver.


Thank you in advance!