Estimated_reflectance and range_sigma in VL53L5 and L8
I have questions regarding estimated_reflectance and range_sigma in VL53L5 and L8
- The reflectance: how is it calculated? Is it R=signal_rate_per_spads*depth^2/K? the number_of sapds_enabled seems a useless parameter for a user? Can we know this calibrated constant K?
- The ambient_light has nothing to do with the R calculation?
- For these multi zone TOF, if we place a flat target in front of TOF, it shall give the same R. ST’ already does the internal compensation for the depth and for the angle of incidence. Right?? I can not find this kind of info in ST’s doc. Can only guess. If it has, please point out the Docs source
- The range_sigma: for L5, if the resolution is 4 x 4, the readout is zero. I can read out this parameter if it is 8 x8
- What is the default sigma_threshold for distance in L5? Is it the same for resolution 8x8 and 4 x4? Also, when I change this threshold, it is unclear if this threshold, e.g.,100mm shall multiply with a scale factor 128. Please confirm that
Thanks in advance if ST or anyone can give me the answers!