Skip to main content
Associate
April 4, 2026
Question

GUI Error with Camera 16GZMAI

  • April 4, 2026
  • 2 replies
  • 188 views

Hi,

I am experiencing a technical issue with the ST 16GZMAI camera when connected to the EVK-U0I1 control board.

While the system works fine with my 55G1MBI1 camera, the EVK GS 1.1.2 GUI fails to recognize this specific model and displays the following error:

"Error: could not broadcast input array from shape (341,280) into shape (340,280)"

I am also unable to change the detector format. Could you please refer me to a technical expert who can assist with the configuration of this model?

Best regards,

Sean

2 replies

April 5, 2026

It sounds like you’re facing a frustrating issue with your ST 16GZMAI camera and the EVK-U0I1 control board. The error message you’re seeing suggests that there might be a mismatch in the expected input dimensions, which can occur if the camera's output format isn't compatible with what the https://tropical-casino.com/ GUI expects.

ST Employee
April 9, 2026

Hi @SeanF ,

This is a known bug; it has already been fixed and will be soon released in the next GUI version.

I will let you know as soon as the new GUI is available.

Sry for the troubles,

Best regards,

Jean 

SeanFAuthor
Associate
April 26, 2026

Hi again,
I wanted to ask if there’s any update on when the updated GUI version will be released. I need to use this camera for my degree project, so I’d really appreciate any timeline you can share.