Has anyone tested the VL53L1X to measure pastures? (pointing down, outdoors, with sunlight from 14 to 93.6 klux)
I´m using multiple sensors for distance ( 3 VL53L1X, 1 HC-SR04, 1 TFMini Plus).
I think I need a lot of coverage to shade the measurement point and thus reduce the light to 140 lux (stable in the lab).
I tried to switch to short mode and time budget to 200ms but that didn't solve my problem.
In the laboratory, the TF mini Plus (850nm) did not generate interference on the VL53L1X (940 nm VCSEL).
I ran the experiments for 3 days over several hours, collecting 8622 + 5450 + 1540 measurements, with only 33% useful data from the VLs, 89% from TF and 95 from HC-SR04.
Does anyone have a better idea?
Looks like the VL53L1X is from "Wayne Enterprises, Inc." It's made for Batman... high tech, exclusive use in the dark. :> I like the features of the VL53L1X. Low cost, low consumption, small size and high sensitivity.