Solved
How do I verify I have my I2C configured correctly for the VL53L5CX?
..
..
Here is a function. Put it at the top of your program. When it runs correctly, you can remove it secure that your I2C is not byte or word swapped.
/* --------------------------------------------------
* --- This function can be used to test VL53L5CX I2C
* --------------------------------------------------
*/
uint8_t vl53l5cx_test_i2c(VL53L5CX_Configuration *p_dev){
uint8_t status = VL53L5CX_STATUS_OK;
printf("Starting VL53L5CX I2C test...\n");
/* To check the I2C RdByte/WrByte function :
* Inside the function “vl53l5cx_is_alive()�?, it will call I2C RdByte/WrByte to
* read device and verion ID. which can help you to verify the I2C RdByte/WrByte
* functions at same time.
*/
uint8_t device_id, revision_id;
status |= WrByte(&(p_dev->platform), 0x7fff, 0x00);
status |= RdByte(&(p_dev->platform), 0, &device_id);
status |= RdByte(&(p_dev->platform), 1, &revision_id);
status |= WrByte(&(p_dev->platform), 0x7fff, 0x02);
if(status)
{
printf("Error Rd/Wr byte: status %u\n", status);
return status;
}
/* To check the I2C RdMulti/WrMulti function:
* Below is example codes which can help you vefify the I2C RdMulti/WrMulti
* function.
*/
uint8_t Data_write[4]={0x5A,0xA5,0xAA,0x55};
uint8_t Data_read[4]={0,0,0,0};
uint8_t Data_default[4]={0,0,0,0};
status |= RdMulti(&(p_dev->platform), 0x100, Data_default, 4);
if(status)
{
printf("Error RdMulti: status %u\n", status);
return status;
}
printf("Read default value and save it at begging\n");
printf("Data_default (0x%x)\n", Data_default[0]);
printf("Data_default (0x%x)\n", Data_default[1]);
printf("Data_default (0x%x)\n", Data_default[2]);
printf("Data_default (0x%x)\n", Data_default[3]);
status |= WrMulti(&(Dev.platform), 0x100, Data_write, 4);
if(status)
{
printf("Error WrMulti: status %u\n", status);
return status;
}
printf("Writing values 0x5A 0xA5 0xAA 0x55\n");
status |= RdMulti(&(p_dev->platform), 0x100, Data_read, 4);
if(status)
{
printf("Error RdMulti: status %u\n", status);
return status;
}
printf("Reading:\n");
printf("Data_read (0x%x)\n", Data_read[0]);
printf("Data_read (0x%x)\n", Data_read[1]);
printf("Data_read (0x%x)\n", Data_read[2]);
printf("Data_read (0x%x)\n", Data_read[3]);
status |= WrMulti(&(Dev.platform), 0x100, Data_default, 4);
printf("Write back default value\n");
if(status)
{
printf("Error WrMulti: status %u\n", status);
return status;
}
status |= RdMulti(&(Dev.platform), 0x100, Data_default, 4);
if(status)
{
printf("Error RdMulti: status %u\n", status);
return status;
}
printf("Read value again to make sure default value was correct loaded\n");
printf("Data_default (0x%x)\n", Data_default[0]);
printf("Data_default (0x%x)\n", Data_default[1]);
printf("Data_default (0x%x)\n", Data_default[2]);
printf("Data_default (0x%x)\n", Data_default[3]);
printf("I2C test done - everything works fine.\n");
return status;
}Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.