How large is the Fov of L5's single-zone?
Hi,
I am doing extrinsic calibration for VL53L5 and a RGB camera, i.e., i need to locate L5's zones in the RGB image (a zone can be representaed by a quadrilaterals in the RGB image after projection).
And my question is: How should i understand the multi-zone of L5?
(1) Do they divide the FoV equally without overlap so each zone has precisely 63/8 degree (for 8x8 zone mapping)?
(2) Or do they occupy same area in the sensor board, so the corner zone cover smaller FoV whie the center zone cover larger FoV?