How to make the VL53L8CH to get data with 64 zones with 18 bins at 15 Hz?
Currently I connected the X-NUCLEO-53L8A1 to F401RE, and I notice that on the web page of VL53L8CH, the sensor can get the data with 64 zones with 18 bins at 15 Hz. But when I use the VL53L8CH with the Example_12_cnh_data which use VL53LMZ_ULD_API, I found that when I set the cnh config to get the data with 64 resolution, 16 bins, and 15Hz, the fps I get from the serial port is only 3.6Hz, not 15Hz. Is there any way to improve the FPS of the code?