Question
How to reduce vl53l5cx_init() timing footprint?
uint8_t vl53l5cx_init(
VL53L5CX_Configuration *p_dev)
{
uint8_t tmp, status = VL53L5CX_STATUS_OK;
uint8_t pipe_ctrl[] = {VL53L5CX_NB_TARGET_PER_ZONE, 0x00, 0x01, 0x00};
uint32_t single_range = 0x01;
...
status |= WrByte(&(p_dev->platform), 0x000F, 0x40);
status |= WrByte(&(p_dev->platform), 0x000A, 0x01);
status |= WaitMs(&(p_dev->platform), 100);
/* Wait for sensor booted (several ms required to get sensor ready ) */
status |= WrByte(&(p_dev->platform), 0x7fff, 0x00);
status |= _vl53l5cx_poll_for_answer(p_dev, 1, 0, 0x06, 0xff, 1);
status |= WrByte(&(p_dev->platform), 0x000E, 0x01);
status |= WrByte(&(p_dev->platform), 0x7fff, 0x02);There is a 100ms fixed delay in the vl53l5cx_init() function.
I am supposing that this delay could be reduced to the strinctly minimum required for SW reboot.
It could be replaced with a polling function like _vl53l5cx_poll_for_mcu_boot or _vl53l5cx_poll_for_answer or a custom one?
Thank you