How to use the VL53L5CX with indirect sunlight
HI,
We have an application where the VL53L5CX is used near a door that are indirectly exposed to sunlight.
I try to be able to do some measurement around 1m. Indoor, the sensor is working good. If I put the sensor near an exterior door, I see some of the cell get values, but most of them have a statuses of 255 or 12.
What's is the maximum ambient light value to have a working sensor ? (the ambient value from the sensor reading).
How we should interpret the SignalPerSpad ?
The sensor is facing face down from the top of the door on the inside side. So the sensor is not directly exposed on the sun.
Is there config values that we can change to add a bit more sunlight noise ?