improve efficiency of VL53L8CX sensor under direct sunlight ?
Hello, I am using this sensor for a project where it is mounted on a cane to detect overhanging objects that could hit visually impaired people. This works fine indoors, but outdoors, when the ambient light is around or greater than 10k Lux—and keeping in mind the sensor is pointed upwards and hit directly by sunlight—it only catches obstacles when they are very close. I am currently using a 4x4 resolution with continuous ranging at 30Hz. My question is: is there a way to increase its efficiency? By efficiency, I mean increasing the detection distance through hardware, structural, or software solutions.