Question
Integration of multiple VL53L0X
- August 6, 2024
- 1 reply
- 1412 views
Dear ST,
I am looking for a solution with the integration of multiple ToFs such as VL53L0x
Objective:
1. Find the distance between the ToF_x(emission only) and ToF_master(reception only)
As the reception zone of vl53l0x is 25 degrees , either one or multiple ToFs could be detected with distance
(NOTE : During operation either of ToF_x will be in linear movement to fall in reception zone )
Setup:
ToF_1 ToF_2 ToF_3 ToF_4
| |
| |
| |
ToF_master
Questions:
1. Do we have the provisions in firmware to control the vl53l0x emission and reception part separately ?
2. Open to explore other ToFs as well helping to solving this solve this issue asap
Please refer attached image for setup idea
Thanks