Interrupt modes via GPIO VL53L3CX
We are using part number VL53L3CX on the X-NUCLEO-53L3A2 board, and one feature we were expecting, for example, is for the sensor to generate an interrupt via configurable GPIO in the following situations:
it is inside or outside a measurement window,
above a measurement.
below a measurement.
By default, this interrupt is generated every time a measurement is completed by the sensor.
Is it possible to configure the sensor to generate interrupts only in the situations mentioned above?
If so, can you help us with some examples?
Is there a part number with these functions?
Thanks