Is the VL53L5CX IEC 60825-1:2007 and IEC 60825-1:2014 compliant and harmonized with the DIN EN ? Is there a compliance report available ?
Hello,
Next week I have to assemble and demonstrate my project in my local school. My project includes the VL53L5CX-Satel. Does the VL53L5CX compliant with the DIN EN ? Can you provide me a compliance report wich include all the measured limits of the VL53L5CX to remain within the IEC 60825-1:2007 and IEC 60825-1:2014 norm?
Do I have to labelling the housing with laser class 1 and the IEC relevance notice?
My school project is based in germany.
I look forward to hearing from you
kind regards
Maik H