Question
Is there any kind of document / application note for VL53L5CX available to guide how to calculate the number of sensors required given the ceiling height and the passage width?
We need to understand the best topology / positioning when considering some different situations, for example:
1) passage with of 0.8m with ceiling height of 2,60m
2) passage width 1,5m, ceiling height of 2,60m
3) passage width of 3m with ceiling height of 2,60m
4) passage width of 6m with ceiling height of 3,5m
Thansk
Mauricio